5.2 Simulator Options Selection
Set up simulator options on the simulator property pages of the Project Properties dialog.
- Open the Project Properties dialog by doing one of the following:
- Click on the project name in the Project window and select File>Project Properties.
- Right click on the project name in the Project window and select “Properties”.
- Under “Categories”, click on “Simulator”
- Select property pages from “Options categories”. Click on an option to see its description in the text box below. Click to the right of an option to change it.
Note: Not all options are available for all devices. Check your
device data sheet for details.