5.2.3 UART I/O Options
For devices that have a USART or UART peripheral, set up applicable options. For more on this feature, see Using a USART/UART.
| Enable UART1 IO | Check to enable UART IO. The currently
attached stimulus file will be used as input. Combined with the UART is the ability to use the standard C library IO capability. When the “Enable UART1 I/O” option is checked, the UART1 is used to read data from a file and write data to a file or the output window. |
| Output | If a file is used for the output, click “File”. If the Output window is to be used for output, click “Window”. |
| Output file | Enter a name for the output file. |