Configure RMON History table on the RMON History Configuration page. The entry index key is ID.Figure 4-40. RMON History Configuration
The RMON History Configuration page has the following parameters:
Delete: Check to delete the entry. It is deleted during the next save.
ID: Indicates the index of the entry. The range is from 1–65535.
Data Source: Indicates the port ID, which is to be monitored. If in stacking switch, the value must add 1000000*(switch ID-1). For example, if the port is switch 3 port 5, then the value is 2000005.
Interval: Indicates the interval in seconds for sampling the history statistics data. The range is from 1–3600 and the default value is 1800s.
Buckets: Indicates the maximum data entries associated with this History control entry stored in RMON. The range is from 1–3600 and the default value is 50.
Buckets Granted: The number of data is saved in the RMON.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.