4.10.1.7.4 Switch-RMON-Event Configuration
Configure the RMON Event table on the RMON Event Configuration page, as shown in the following figure. The entry index key is ID.

The RMON Event Configuration page has the following parameters:
- Delete: Check to delete the entry. It is deleted during the next save.
- ID: Indicates the index of the entry. The range is from 1–65535.
- Desc: Indicates this event. The string length is from 0–127, default is a null string.
- Type: Indicates the notification of the event. The following are the possible types.
- None: No SNMP log is created; no SNMP trap is sent
- Log: Create SNMP log entry when the event is triggered
- Snmptrap: Send SNMP trap when the event is triggered
- Logandtrap: Create SNMP log entry and sent SNMP trap when the event is triggered
- Event Last Time: Indicates the value of sysUpTime at the time this event entry last generated an event