5.25.6 TSN PSFP Stream Gate Status
The TSN PSFP Stream Gate Status page has the following parameters:
- SGI ID: The Stream Gate Instance parameter is an index into the Stream Gate Table.
- Oper Gate Enabled: The Gate Enabled parameter determines whether the stream gate is active (true) or inactive (false).
- Oper Gate States: The operational value of the Gate States parameter for the stream gate. The open value indicates that the gate is open, the closed value indicates that the gate is closed.
- Cycle Time Numerator: The operational value of the numerator of the Cycle Time parameter for the gate. The numerator and denominator together represent the cycle time as a rational number of seconds.
- Cycle Time Denominator: The operational value of the denominator of the Cycle Time parameter for the gate. The numerator and denominator together represent the cycle time as a rational number of seconds.
- Cycle Time Extension: The operational value of the Cycle Time Extension parameter for the gate. The value is an unsigned integer number of nanoseconds.
- Base Time: The operational value of the Base Time parameter for the gate. The value is a representation of a PTPtime value, consisting of a 48-bit integer number of seconds and a 32-bit integer number of nanoseconds.
- Current Time: The current time, in PTPtime, as maintained by the local system. The value is a representation of a PTPtime value, consisting of a 48-bit integer number of seconds and a 32-bit integer number of nanoseconds. Only the seconds are displayed.
- Config Change Time: The PTPtime at which the next config change is scheduled to occur. The value is a representation of a PTPtime value, consisting of a 48-bit integer number of seconds and a 32-bit integer number of nanoseconds.
- Config Change Error: A counter of the number of times that a re-configuration of the traffic schedule has been requested with the old schedule still running and the requested base time was in the past.
- Tick Granularity: The granularity of the cycle time clock, represented as an unsigned number of tenths of nanoseconds.
- Config Pending: The value of the Config Pending state machine variable. The value is TRUE if a configuration change is in progress but has not yet completed.
- Oper IPV: The operational value of the IPV parameter for the gate. A value of -1 denotes the null value.
- GCL Length: The operational value of the List Max parameter for the gate. The integer value indicates the number of entries (TLVs) in the oper Control List.
- GCL Status: A link to the GCL parameter status.