5.25.5 TSN PSFP Stream Filter Statistics

The TSN PSFP Stream Filter Statistics page has the following parameters:
- Clear: This box is used to mark an entry for clearance in next Clear operation.
- SFI ID: The Max Stream Filter Instances parameter defines the maximum number of stream filter instances that are supported by this Bridge component.
- Matching Frame Count: The Matching Frames Count counter counts received frames that match this stream filter.
- Passing Frame Count: The Passing Frames Count counter counts received frames that pass the gate associated with this stream filter.
- Not Passing Frame Count: The Not Passing Frames Count counter counts received frames that do not pass the gate associated with this stream filter.
- Passing SDU Count: The Passing SDU Count counter counts received frames that pass the SDU size filter specification associated with this stream filter.
- Not Passing SDU Count: The Not Passing SDU Count counter counts received frames that do not pass the SDU size filter specification associated with this stream filter.
- RED Frames Count: The RED Frames Count counter counts received random early detection (RED) frames associated with this stream filter.