5.25.1 TSN Egress Port Frame Preemption Status
The TSN Egress Port Frame Preemption Status page has the following parameters:
- Port: The logical port for the settings contained in the same row.
- Hold Advance: The value of the hold-Advance parameter for the Port in nanoseconds. There is no default value; the hold-Advance is a property of the underlying MAC.
- Release Advance: The value of the release-Advance parameter for the Port in nanoseconds. There is no default value; the release-Advance is a property of the underlying MAC.
- Preemption Active: The value is active (TRUE) when preemption is operationally active for the Port, and idle (FALSE) otherwise.
- Hold Request: The value is hold (TRUE) when the sequence of gate operations for the Port has executed a Set-And-Hold-MAC operation, and release (FALSE) when the sequence of gate operations has executed a Set-And-Release-MAC operation. The value of this object is release (FALSE) on system initialization.
- Status Verify: The status of the MAC Merge sublayer verification for the given device. The possible values are:
- Initial – Verification process is initializing
- idle – The verification process is ongoing
- send – The verification process is ongoing
- wait – The verification process is ongoing
- succeeded – The verification process is completed and frame preemption is supported
- failed – The verification process is completed and frame preemption is not supported
- disabled – Frame preemption is disabled
- indeterminate – The verification process is completed but it cannot be determined whether link partner supports frame preemption
- Loc Preempt support: The value is TRUE when preemption is supported on the port, and FALSE otherwise.
- Loc Preempt Enabled: The value is TRUE when preemption is enabled on the port, and FALSE otherwise.
- Loc Preempt Active: The value is TRUE when preemption is operationally active on the port, and FALSE otherwise.
- Loc Add Frag Size: The value of the 802.3br LocAddFragSize parameter for the port. The minimum size of non-final fragments supported by the receiver on the local port. This value is expressed in units of 64 octets of additional fragment length. The minimum non-final fragment size is: (LocAddFragSize + 1) * 64 octets.