Configure the SNMPv3 view table on the SNMPv3 View Configuration page, as
shown in the following figure. The entry index keys are View Name
and OID Subtree.Figure 4-9. SNMPv3 View Configuration
The SNMPv3 View Configuration page has the following parameters:
Delete: Check to delete the entry. It is deleted during the next save.
View Name: A string identifying the view name belonging to this entry. The allowed string length is 1 to 32 and the allowed content is ASCII characters from 33 to 126.
View Type: Indicates the view type belonging to this entry. Possible view types are:
Included: An optional flag to indicate that this view subtree must be included
Excluded: An optional flag
to indicate that this view subtree must be excluded. In general, if the view
type is excluded, there should be another view entry existing with view type
as included and it's OID subtree should overstep the excluded view
entry.
OID Subtree: The OID defines the root of the subtree to add to the named view. The allowed OID length is 1 to 128. The allowed string content is digital number or asterisk (*).
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.