5.6.9 Command Complete Event
Format:
| Event | Event Code | Event Parameters |
| Command_Complete | 0X0E |
Num_HCI_Command_Packets Command_Opcode Return_Parameters |
Use this event to transmit the return status of a command and the other event parameters that are specified for the issued HCI command. The Num_HCI_Command_Packets event parameter allows the controller to indicate the number of HCI command packets the host can send to the controller. The event parameters are shown in the following figure.
| Example: | 04 0E 04 01 7B 20 00
|
// Command complete event with status parameter |