Firmware Request Approval
The following are the steps for the firmware request approval:
After clicking Connect/Update, a Bluetooth Low Energy link connection is established between the devices, and the firmware update procedure starts.
- The device enters into OTAPC mode, and the central device initiates a firmware update request. The remote side receives the firmware update request as an event.
Figure 8-27. Microchip RNBD Utility Tool OTAPC Tab OTA Update Request The remote device, then, must approve the request with a predefined
OTAA,01command. The remote device receives anAOK<CR><LF>response.Note: The host MCU can send this approval command if the RNBD451 is connected with the host MCU.- After that, the central device starts firmware distribution by sending the firmware files in maximum allowed fragmented size received from the remote device along with the firmware distribution command.
Figure 8-28. Microchip RNBD Utility Tool OTAPC Tab OTA Update Request Approval - The firmware update proceeds from then on. The remote device side continuously receives an OTA updating in progress event.