Scan
The following are the steps to initiate the scan process:
After selecting the firmware file, click Scan to initiate a scanning from the selected central device to capture the nearby peripheral devices.
- Like the guidance displayed in the message Console tab, after clicking the Scan, the user must wait for 10 seconds for the central device to complete the scanning.
Figure 8-25. Microchip RNBD Utility Tool OTAPC Tab Scan Select Upon completion of the scanning, the table is filled with the scan result.