Firmware Update in Progress
- During the firmware update, the below mentioned information will display on the tool.
Figure 8-29. Microchip RNBD Utility Tool OTAPC Tab Remote Device Firmware Update in Progress - Progress label that displays the percentage of completion
- Live Progress bar update view
- Status label displays the current status
- Total bytes completed
- Background update station on console text view
- After completion, the tool updates the following:
- A message box displaying the DFU update completion. Press OK to proceed.
- Progress indicator shows 100%
- Status changes to DFU Update Completed!
- Bytes completed matches with the total bytes
- A Firmware Distribution Complete message on the console text log
Figure 8-30. Microchip RNBD Utility Tool OTAPC Tab Remote Device Firmware Update Complete - A message box displays the DFU update completion. Press OK to proceed.
- Progress indication shows 100%
- Status changes to DFU Update Completed!
- Bytes completed matches with the total bytes
- A Firmware Distribution Complete message on the console text log
- Upon pressing OK on the message box, the total time taken for the firmware update will be displayed on console text log.
Figure 8-31. Microchip RNBD Utility Tool OTAPC Tab Remote Device Firmware Update Time Complete