23.6.3.4 Function system_pinmux_group_set_output_strength()
Configures the output driver strength mode for a group of pins.
void system_pinmux_group_set_output_strength( PortGroup *const port, const uint32_t mask, const enum system_pinmux_pin_strength mode)
Configures the output drive strength for a group of pins, to control the amount of current the pad is able to sink/source.
| Data direction | Parameter name | Description |
|---|---|---|
[in] | port |
Base of the PORT module to configure |
[in] | mask |
Mask of the port pin(s) to configure |
[in] | mode |
New output driver strength mode to configure |