2.46.9 FCW_ErrorGet Function
C
FCW_ERROR FCW_ErrorGet( void )
Summary
Returns the error state of FCW controller.
Description
This function returns the erorr status of the last FCW operation.
Precondition
None.
Parameters
None
Returns
Return FCW_ERROR type of value. In case of error, this value can be a combination of multiple and different error conditions.
Example
if(FCW_ErrorGet() != FCW_ERROR_NONE)
{
// The error status can indicate multiple error conditions.
if(FCW_ErrorGet() & (FCW_ERROR_WRITE | FCW_ERROR_RESET))
{
// There are multiple error conditions.
}
}
Remarks
None.