2.88.8 PTG_StepSequenceStart Function
C
void PTG_StepSequenceStart(void)
Summary
Starts the step sequence of the PTG peripheral of the device.
Description
This function initiates the step sequence for the PTG peripheral of the device. This process begins the programmed sequence of operations. Ensures the device performs Step Commands in the correct order.
Precondition
The PTG peripheral must have been enabled using the PTG_Enable API. The Step Sequence configurations should be carefully made in the Configuration Options GUI. This function should be called when the PTG peripheral is required to start the step sequence.
Parameters
None.
Returns
None.
Example
PTG_Initialize(); PTG_Enable(); PTG_StepSequenceStart();
Remarks
None.