2.88.5 PTG_Initialize Function
C
void PTG_Initialize(void)
Summary
Initializes PTG peripheral of the device.
Description
This function initializes the PTG Peripheral Library (PLIB) of the device with the values configured in the Configurations Options GUI. Once the peripheral is initialized, Step Sequence APIs can be used to start the Step Sequence.
Precondition
MCC GUI should be configured with the correct values.
Parameters
None.
Returns
None.
Example
void main(void) { PTG_Initialize(); PTG_Enable(); PTG_StartStepSequence(); while (1) { PTG_SoftwareTriggerSet(); bool wdtBit = PTG_WatchdogTimeoutStatusGet(); if(wdtBit){ PTG_StepSequenceStop(); PTG_Disable(); } } }
Remarks
None.