2.88.2 PTG_Disable Function
C
void PTG_Disable(void)
Summary
Disables the PTG peripheral of the device.
Description
This function disables the PTG Peripheral Library (PLIB) of the device, for its desired use.
Precondition
The PTG peripheral must have been initialized using the PTG_Initialize API. The peripheral should be enabled using the PTG_Enable() API. This function should be called when the PTG peripheral is required to disable.
Parameters
None.
Returns
None.
Example
PTG_Disable();
Remarks
None.