2.96.18 RNG_NumGen2Get Function
C
uint32_t RNG_NumGen2Get (void);
Summary
Returns the value in the RNGNUMGEN2 register.
Description
When the PRNG operation is finished, RNGNUMGEN2 register contains the MSB 32-bits of the current random number in the PRNG. This function can be used to read the generated random number.
Precondition
None.
Parameters
None.
Returns
The MSB (32-bits) of the pseudo-random number generated in PRNG.
Example
uint32_t numgen2 = 0;
numgen2 = RNG_NumGen2Get();
Remarks
None.