2.96.6 RNG_Seed2Get Function
C
uint32_t RNG_Seed2Get (void);
Summary
Returns the content of RNGSEED2 register.
Description
This function is used to read the Most Significant Byte 32-bits of the TRNG number (from RNGSEED2 register).
Precondition
RNG_Initialize must have been called before using this function.
Parameters
None.
Returns
Contents of RNGSEED2.
Example
uint32_t seed2 = 0;
seed2 = RNG_Seed2Get();
Remarks
Use together with RNG_Seed1Get() if the required bits length is more than 32-bits.