2.132.13 WDT_IsWindowEnabled Function
C
bool WDT_IsWindowEnabled(void);
Summary
Checks if the window mode of the Watchdog Timer is enabled.
Description
This function checks if the window mode of the Watchdog Timer is enabled.
Preconditions
None.
Parameters
None.
Returns
bool - true if window mode is enabled, false if disabled.
Example
bool isWindowEnabled = WDT_IsWindowEnabled();
Remarks
None.