4.6.2 Node UWB Configuration
To ensure proper functionality, the user must correctly configure each node type
participating in the UWB demonstration. After start-up, the state of the UWB parameter
configuration on the selected node is read and displayed in the status bar at the bottom
of the GUI. The following are the three possible states:
- Valid: The parameter settings on the selected node are valid.
- Parameter Settings Invalid: The parameter settings on the selected node are invalid. No measurement can be done. Set up a proper configuration for the selected node. For more details, refer to Parameter Settings.
- No Memory available: No memory is available to read the parameter settings from or to write it to. No measurement can be done.