4.7.2.3.5 Radio Group
The Radio Group widget is a group of radio buttons where only one option can be selected at any time. Initially the first option is selected.

To make changes to the list, use the editor under Values.

You can also display the options horizontally.
Data Fields
The Radio Group widget has a source data field. Each time the state of the widget is changed a value is sent.
Configuration
Hover over parameters in visualizer for more information.
| Parameter | Type | Usage |
|---|---|---|
| Values | Editor | Edit a list of options to name, add, delete or rearrange options. |
| Horizontal | Check box | Check to display options horizontally. |
| Parameter | Type | Usage |
|---|---|---|
| Font Size | Numeric | Enter font size |
| Font Weight | Dropdown box | Select the font weight (such as bold) |
| Font Style | Dropdown box | Select the font style (such as italics) |
| Font Family | Dropdown box | Select the font family (such as segment) |