7.1.3 Document Conventions
This document uses the following conventions:
- Information input by the user follows this format: keyboard input
- The contents of a file follows this format: file contents
This document uses the following variables:
- Actel FPGA family libraries are shown as <act_fam>. Substitute the desired Actel FPGA family Fusion, IGLOOTM/e, ProASIC3/E, ACT1, ACT2 (for ACT 2 and 1200XL devices), ACT3, 3200DX, MX, SX, SX-A, eX, Axcelerator, A500k, and APA as needed. For example, edn2vhdl fam:<act_fam> <design_name>.
- Compiled VHDL libraries are shown as <vhd_fam>. Substitute <vhd_fam> for the desired VHDL family Fusion, IGLOO/e, ProASIC3/E, ACT1, ACT2 (for ACT 2 and 1200XL devices), ACT3, A3200DX, MX, SX, SX-A, eX, Axcelerator, A500k, and APA as needed. The VHDL language requires that the library names begin with an alpha character.