7.2.2 System Setup

After installing Powerview, make sure you set the proper environment variables in your UNIX shell script. The following are C-shell variables. If you are using another shell, adjust the syntax accordingly.

setenv WORKVIEWHOME <ePD_install_directory>
setenv ALSDIR <actel_install_directory>
setenv WDIR <powerview_install_directory>
set path=($ALSDIR/bin $path)
set path=($WORKVIEWHOME/bin $path)

For example:

WORKVIEWHOME/ax_1/viewlogic/ePD10/epd/I-O/common/sun05551

If you use SunOS or Solaris, you must also set the following variable:

setenv LD_LIBRARY_PATH $ALSDIR/lib

If you use HP-UX, you must also set the following variable:

setenv SHLIB_PATH $ALSDIR/lib

If you use SpeedWave, you must also set the following variable:

setenv VANTAGE_VSS <vantage_install_directory>

For more information about setting environment variables, see the Designer User’s Guide and the Innoveda documentation.