2.10.1.2 “Events” Event Byte
The “events” event byte is located in the R14 AVR register.
| Event | Description |
|---|---|
| IDCHKA | This flag is set if the ID check was successful during reception on path A. |
| WCOKA | This flag is set if a wake check OK event was detected on path A. |
| SOTA | This flag is set if a start of telegram event was detected on path A. |
| EOTA | This flag is set in RXMode/PollingMode if an end of telegram event was detected on path A. This flag is set in TXMode(buffered) if the transmission is completed on path A. |
| IDCHKB | This flag is set if the ID check was successful during reception on path B. |
| WCOKB | This flag is set if a wake check OK event was detected on path B. |
| SOTB | This flag is set if a start of telegram event was detected on path B. |
| EOTB | This flag is set in RXMode/PollingMode if an end of telegram event was detected on path B. This flag is set in TXMode(buffered) if the transmission is completed on path B. |