2.9.9 Register Refreshing

A register refreshing process can be used to force the reload of the complete service/channel configuration of the SRAM currentService structure using its default EEPROM or SRAM configuration the next time a data transmit or receive mode ramps up. This can be useful in these circumstances:

  • In a polling scenario where only one service with different channels is used and the user wants a periodic refresh of the currentService data in the SRAM with the data from the EEPROM service configuration
  • If an SRAM service configuration is updated via SPI and the user wants to transfer these changes to the currentService structure at the subsequent start-up of a receive or transmit mode
  • If the currentService was manipulated by the user and the default EEPROM/SRAM configuration needs to be reloaded
Note: If a receive or transmit mode is started with a service that differs from the service in the currentService structure, the complete service/channel configuration in currentService is updated in any case (see Service-Based Concept).

A register refreshing process can be triggered at the following time points:

  • During the periodic self-check in PollingMode or during a self-check that is started by using the “Calibrate and Check” SPI command if enabled in eepTrxCal.calConf1.EN_REGREFRESH.
Address Name Bit 7 Bit 6 Bit 5 Bit 4 Bit 3 Bit 2 Bit 1 Bit 0
0x001C calConf1 —EN_TEMP_MEAS EN_SRCCAL EN_FRCCAL ———EN_REGREFRESH
Note: No SPI command directly supports a register refresh. Refreshing the register is only available in combination with the system self-check and calibration procedure.

The register refresh procedure requires additional time, see Timing Characteristics.