1.7 Programming the Device
(Ask a Question)The following steps describe how to program the device on a PolarFire Evaluation Kit.
Ensure that the following jumper settings are followed.
Important: Power-down the board before making the jumper connections.Table 1-2. Jumper Settings For Evaluation Kit Jumper Description J46 Short pin 1 and 2 to set the Reference Clock to 125 MHz on-board oscillator J18, J19, J20, J21, and J22 Short pin 2 and 3 to program the PolarFire FPGA through FTDI J28 Short pin 1 and 2 to program through the on-board FlashPro5 J4 Short pin 1 and 2 for manual power switching using SW3 J17 Short pin 1 and 2 J12 Short pin 3 and 4 for 2.5V - Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the Host PC to the J5 connector (FTDI port) on the board.
- Power on the board using the SW3 slide-switch.
- Switch OFF the DIP1 switch.
- Connect TXN to RXN and TXP to RXP using two SMA to SMA cables, as shown in the following figure. The following figure shows the board setup.
Figure 1-12. Board Setup (Evaluation kit) - In the Design Flow window, select Run PROGRAM Action, as shown in the following figure. This programs the design into the device.
Figure 1-13. Programming the Device