A Libero® SoC project with FHB enabled is created using the
TCL script. A TCL script is provided in the design files folder in the HW
directory to create a Libero SoC Project with FHB enabled.
To create the Libero project with FHB enabled, perform the following steps:
Launch Libero SoC.
Select Project > Execute Script.....
Select Browse and
then select script.tcl from the downloaded HW
directory.
In the Argument
tab, provide the FHB_ENABLE argument.
Click Run.
After successfully executing the TCL script, the Libero SoC project is created
within the HW directory. To confirm that the FHB is enabled, navigate to Project > Project Settings and verify that the Enable FPGA Hardware Breakpoint Auto
Instantiation option is selected, as shown in the following figure.Figure 1-11. Enabling FHB
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.