1.3 Demo Design
(Ask a Question)This section describes the fabric, DDR interface, and XCVR design blocks implemented in Libero SoC.
The following figure shows the top-level blocks of SmartDebug.
Important: The FHB feature is not enabled in the demo design. To enable FHB debugging, provide the “FHB_ENABLE” argument with the given TCL script. This creates the design without the DDR controller block, because FHB debugging is currently not supported for designs that include a DDR controller. For more information about enabling FHB debugging using the TCL script, see Appendix 4: Running the TCL Script.
The top level block contains the following blocks: