2.5.5.11 Calibration Command
The configuration command (CAL) is used to automatically calibrate the board. It requires accurate and stable voltage and current sources and loads, which can be provided by a meter test bench like the WECO (or equivalent equipment). Refer to Calibrate the Demo Board Using the Demo Meter Application for additional information.
This command must be sent after a configuration command, to ensure that the proper configuration was applied.
There are four variants of the calibration command:
- CAL_A to calibrate the phase A individually
- CAL_B to calibrate the phase B individually
- CAL_C to calibrate the phase C individually
- CAL_T to calibrate a three phases system simultaneously
The configuration command has the following parameters:
- The CAL_A, CAL_B, and CAL_C
commands:
- Ua (for “CAL_A), Ub (for “CAL_B), Uc (for “CAL_C): Rms voltage applied to the voltage input. Units: Volts
- Ia (for “CAL_A), Ib (for “CAL_B), Ic (for “CAL_C): Rms current applied to the current input. Units: Amps
- Aa (for “CAL_A), Ab (for “CAL_B), Ac (for “CAL_C): Angle between the voltage and current vectors. Units: Degrees. The value is positive if the current is lagging the voltage
- The CAL_T command:
- Ua: Rms voltage applied to the voltage input (phase A). Units: Volts
- Ub: Rms voltage applied to the voltage input (phase B). Units: Volts
- Uc: Rms voltage applied to the voltage input (phase C). Units: Volts
- Ia: Rms current applied to the current input (phase A). Units: Amps
- Ib: Rms current applied to the current input (phase B). Units: Amps
- Ic: Rms current applied to the current input (phase C). Units: Amps
- Aa: Angle between the voltage and current vectors (phase A). Units: Degrees. The value is positive if the current is lagging the voltage.
- Ab: Angle between the voltage and current vectors (phase B). Units: Degrees. The value is positive if the current is lagging the voltage.
- Ac: Angle between the voltage and current vectors (phase C). Units: Degrees. The value is positive if the current is lagging the voltage.
The maximum resolution available is 0.001V (voltages), 0.0001A (currents), 0.001º (angles) and 0.01 Hz (frequency).
Examples:
- Calibrate phase A, applying 220.00V, 5.000A, angle = 60.00º: “CAL_A (Ua = 220.00, Ia = 5.000, Aa = 60.00)”
- Calibrate phase B, applying 230.00V, 10.000A, angle = 60.00º: “CAL_B (Ub = 230.00, Ib = 5.000, Aa = 60.00)”
- Calibrate phase C, applying 120.00V, 1.000A, angle = 60.00º: “CAL_C (Uc = 120.00, Ic = 1.000, Aa = 60.00)”
- Calibrate a three phases system, applying to all phases 220.00V, 5.000A and a phase shift of 60.00º: “CAL_T (Ua = 220.00, Ia = 5.000,Aa = 60.00, Ub = 220.00, Ib = 5.000, Ab = 60.00, Uc = 220.00, Ic = 5.000, Ac = 60.00)”