1.1.12.2 WDRV_WINC_APStart Function
WDRV_WINC_STATUS WDRV_WINC_APStart (
DRV_HANDLE handle,
const WDRV_WINC_BSS_CONTEXT *const pBSSCtx, const WDRV_WINC_AUTH_CONTEXT *const pAuthCtx,
const WDRV_WINC_HTTP_PROV_CONTEXT *const pHTTPProvCtx, const WDRV_WINC_BSSCON_NOTIFY_CALLBACK pfNotifyCallback
)
C
Summary
Starts an instance of Soft-AP.
Description
Using the defined BSS and authentication contexts with an optional HTTP provisioning context (socket mode only) this function creates and starts a Soft-AP instance.
Precondition
WDRV_WINC_Initialize should have been called. WDRV_WINC_Open should have been called to obtain a valid handle. A BSS context must have been created and initialized. An authentication context must have been created and initialized.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_WINC_Open. |
pBSSCtx | Pointer to BSS context. |
pAuthCtx | Pointer to authentication context. |
pHTTPProvCtx | Pointer to HTTP provisioning context (optional). |
pfNotifyCallback | Pointer to notification callback function. |
Returns
WDRV_WINC_STATUS_OK - The request has been accepted. WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open. WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect. WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected. WDRV_WINC_STATUS_INVALID_CONTEXT - The BSS context is not valid.
Remarks
None.