1.1.8.10 WDRV_WINC_IPUseDHCPGet Function
bool WDRV_WINC_IPUseDHCPGet(DRV_HANDLE handle)
C
Summary
Determine if DHCP is to be used.
Description
Determines if the WINC will use DHCP for IP address configuration.
Precondition
WDRV_WINC_Initialize should have been called. WDRV_WINC_Open should have been called to obtain a valid handle. The WINC must not be connected.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_WINC_Open. |
Returns
Flag indicating if DHCP will be used.
Remarks
Only applicable when connected in infrastructure station mode.