1.1.8.7 WDRV_WINC_IPDHCPServerConfigure Function
WDRV_WINC_STATUS WDRV_WINC_IPDHCPServerConfigure (
DRV_HANDLE handle, uint32_t ipAddress, uint32_t netMask,
WDRV_WINC_DHCP_ADDRESS_EVENT_HANDLER const pfDHCPAddressEventCallback
)
C
Summary
Configures the Soft-AP DHCP server.
Description
Configures the IPv4 address and callback for the DHCP server.
Precondition
WDRV_WINC_Initialize should have been called. WDRV_WINC_Open should have been called to obtain a valid handle. The WINC must not be connected.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_WINC_Open. |
ipAddress | IPv4 address. |
netMask | IPv4 netmask. |
pfDHCPAddressEventCallback | Callback for DHCP address events. |
Returns
WDRV_WINC_STATUS_OK - The request has been accepted. WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open. WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect.
Remarks
Only applicable when connected in Soft-AP mode. Parameter netMask is only applicable for WINC drivers supporting the extended Soft-AP API m2m_wifi_enable_ap_ext and m2m_wifi_start_provision_mode_ext.