1.1.5.2 WDRV_WINC_BSSFindFirst Function
WDRV_WINC_STATUS WDRV_WINC_BSSFindFirst (
DRV_HANDLE handle, WDRV_WINC_CHANNEL_ID channel, bool active,
const WDRV_WINC_SSID_LIST *const pSSIDList,
const WDRV_WINC_BSSFIND_NOTIFY_CALLBACK pfNotifyCallback
)
C
Summary
Request a BSS scan is performed by the WINC.
Description
A scan is requested on the specified channels. An optional callback can be provided to receive notification of the first BSS discovered.
Precondition
WDRV_WINC_Initialize must have been called. WDRV_WINC_Open must have been called to obtain a valid handle.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_WINC_Open. |
channel | Channel to scan, maybe WDRV_WINC_ALL_CHANNELS or WDRV_WINC_CID_ANY in which case all enabled channels are scanned. |
active | Use active vs passive scanning. |
pSSIDList | Pointer to list of SSIDs to match on. |
pfNotifyCallback | Callback to receive notification of first BSS found. |
Returns
WDRV_WINC_STATUS_OK - A scan was initiated.
WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open. WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected. WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect.
WDRV_WINC_STATUS_SCAN_IN_PROGRESS - A scan is already in progress.
Remarks
If channel is WDRV_WINC_ALL_CHANNELS or WDRV_WINC_CID_ANY then all enabled channels are scanned. The enabled channels can be configured using WDRV_WINC_BSSFindSetEnabledChannels. How the scan is performed can be configured using WDRV_WINC_BSSFindSetScanParameters.