31.1.10.2 Boot Write Protect
Write protection also includes erase protection
The BWP registers are used to write/erase protect individual pages within BFM. The protect bits are grouped into Lower Boot (LBWPn) and Upper Boot (UBWPn). These are two equal size regions containing the same number of pages. BWP always uses the logical page location which depends on BFSWAP to control protection for the physical page.
At reset, all BWP bits are set to logic ‘1’, write protecting all user accessible BFM pages. Clearing a BFM page bit within its register removes write protect from the corresponding page.
See the Interrupt Flag Summary Table for the effects of write protect errors on INTFLAG.
BWP Lock/Unlock Sequence
LBWP and UBWP require a lock/unlock sequence as described in SFR Write Unlock Values. Any attempt to write to these registers when locked will have no effect.
Local Lock Bits
The user may optionally select to prevent further writes to a BWP register by also setting the local LOCK bit (in the same register) when writing the BWP value.
When the local lock bit is set (LOCK = 1), subsequent writes to that register (even if the unlock sequence is followed) have no effect, creating a “write once’ register. The local LOCK bit reverts to the unlocked state at reset.
See Lower (LBWP) and Upper (UBWP) BFM Write Protect Registers for all possible settings regarding the lock and protection bits.