3.3.4.19 EMAFE_SetComparisonModeChannelB Function
C
void EMAFE_SetComparisonModeChannelB ( EMAFE_COMPARISON_DATA *data );Summary
Set the comparison mode between channel B and two thresholds.
Description
This feature compares one channel with two thresholds. A comparison event is triggered as a result of the combination of two events.
The first event is triggered when the channel data is lower than the first threshold, whereas the second event is triggered if the channel data is greater than the second threshold. The combination can be defined as an “or” or “and” between the two events.
Therefore, the comparison can detect if the channel data is out of range, in range or higher or lower than a threshold.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| data | Pointer to the configuration values of the channel comparison mode. |
Returns
None.
Example
EMAFE_COMPARISON_DATA chnComparison;
chnComparison.channel = EMAFE_COMP_CHN_2_ID;
chnComparison.condition = EMAFE_CONDITION_OR;
chnComparison.threshold1 = threshold1Value;
chnComparison.threshold2 = threshold2Value;
EMAFE_SetComparisonModeChannelB(&chnComparison);
Remarks