3.3.4.1 EMAFE_Initialize Function

C

void EMAFE_Initialize ( void );

Summary

Initializes given instance of EMAFE peripheral.

Description

This function initializes given instance of EMAFE peripheral of the device with the values configured in MCC GUI. Once the peripheral is initialized, peripheral can be used for capturing samples.

Precondition

MCC GUI should be configured with the right values.

Parameters

None.

Returns

None.

Example

EMAFE_Initialize();

Remarks

This function must be called before any other EMAFE function is called. This function should only be called once during system initialization.