3.4.3 Create NVRAM-based Partition in HSM Module
This step uses the nvram-sw utility to create a storage partition in
non-volatile memory of the HSM module for storing information that must be physically
uncloneable. Figure 3-9 shows output during NVRAM
partition creation.
To run this action:
- The module must be in the operational mode.
- The ACS (admin) cards must be
inserted into the card reader according to the quorum number specified during
creation of the Security World. Enter the following command to create
NRAM:
nvram-sw.exe -a -b 8096 -n udsigner -k seeinteg,userdata-signer
The -b parameter specifies partition size in bytes. The value of 8096 specifies partition size. This value is fixed in the current version of the M-HSM server.
Note: The -k parameter must follow the exact
format: comma separated values with no spaces.