3.4.6 Generate the U-HSM Master Key (g4mcu)
This is a symmetric encryption key that protects all internal project information such as keys, tickets, security protocol data, and so on, while processing inside the U-HSM.
Generate the U-HSM master key as follows:
- Open the command prompt as an administrator and change directory to C:\Microsemi\Tools.
- Execute the following command (see the sample
output in Figure 3-11).
%nfast_home%\python\bin\python.exe" C:\Microsemi\Tools\gensymmkey.py -u userdata-signer-i g4mcu-< CU_MASTER_HSM_UUID >
CU_MASTER_HSM_UUID is a user-selected master key UUID. This UUID must be
set in the settings of the application using this HSM server. Length: 40 hex symbols.
This key must be unique within the Security World used by this HSM.