3.4.7 Set Up the SEE Machine Firmware for Loading into the HSM Module
Different HSM module types require different firmware images. All images are located in the SEE folder and have the extension sar. The userdata.sar file works with any module type.
|
Module Type |
Firmware File |
|---|---|
|
nShield Edge |
M-HSMsee-edg.sar |
|
nShield Solo |
M-HSMsee-ppc.sar |
The next step is to confirm that the SEE Machine firmware has loaded successfully. Use
the GetLoadingSEEName.bat script in the Utils folder, as shown in Figure 3-13.
The SEE Machine firmware is loaded when the ‑MemAllocUser variable
reads a non-zero value.
-MemAllocUser
remains 0.If the module cannot load the firmware, check the correctness of the parameters specified during the loadsee‑setup step and repeat the attempt, making sure the proper module type is selected.