1.1.34.17 WDRV_WINC_WifiCoexConfGet
C
WDRV_WINC_STATUS WDRV_WINC_WifiCoexConfGet
(
DRV_HANDLE handle,
WDRV_WINC_COEX_CFG *pCoexCfg,
bool *pIsEnabled
)Description
Returns the current coexistence arbiter configuration related to interface mode, priority and antenna mode as well as if the arbiter is enabled or not.
Precondition
WDRV_WINC_Initialize must have been called.
WDRV_WINC_Open must have been called to obtain a valid handle.
Parameters
| Parameters | Description |
|---|---|
| handle | Client handle obtained by a call to WDRV_WINC_Open. |
| pCoexCfg | Pointer to structure to receive the coexistence arbiter settings. |
| pIsEnabled | Pointer to a flag to receive the enabled state or the arbiter. |
Returns
- WDRV_WINC_STATUS_OK - The request has been accepted.
- WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open.
- WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect.
- WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected.
- WDRV_WINC_STATUS_RETRY_REQUEST - The request should be retried.
Remarks
pCoexCfg can be NULL if the arbiter settings are not required.
pIsEnabled can be NULL if the arbiter enabled state is not required.