2.4.18 CAN_TP_Tasks()
void CAN_TP_Tasks (void )
Tasks routine that keeps the CAN-TP layer running.
This should be called frequently to keep the CAN-TP layer running correctly.
This needs to be called at least as frequently as the minimum CAN-TP timeout of the system which is typically at least once a second (though more frequent is preferred).CAN_TP_Initialize function should have been called before calling this function. |
None |