2.4.5 CAN_TP_EventCallbackSet()
void CAN_TP_EventCallbackSet (CAN_TP_EventCallback callback)
Sets and event callback handler for the CAN-TP events to go to.
The specified function will be called whenever there are events that the ISO 15765-2 specification says the upper layer should be notified.
This is typically called in the system configuration and will not be used during the normal operation.
-
The event of CAN_TP_EVENT type
-
The addressing information in the CAN_TP_SERVICE_HEADER struct
-
The event data payload in the *void pointer
The event data payload will be a pointer to a structure that has the data for that specific type of event. For example, the CAN_TP_EVENT_INDICATION event will use the CAN_TP_EVENT_INDICATION_DATA structure for the data field.
CAN_TP_Initialize function should have been called before calling this function. |
| in | callback |
Function to call on an event. |
None |