2.4.12 CAN_TP_MessageSend()
bool CAN_TP_MessageSend (const uint8_t * buffer, size_t length)
Sends a given message using CAN-TP.
Sends the specified message through the CAN-TP layer.
CAN_TP_Initialize function should have been called before calling this function. |
| in | buffer |
Pointer to a message to send. |
| in | length |
Length of the message to send. |
bool - true if able to start sending message, false if couldn't start |