2.4.3 CAN_PHY_Transmit()
bool CAN_PHY_Transmit (uint32_t messageId, bool isEid, uint8_t * data, uint8_t length)
Adaptor method that interfaces with the CAN/CAN-FD method Transmit.
CAN/CAN-FD Initialize function should be called before calling this function. |
| in | messageId |
ID of the message to send over CAN/CAN-FD. |
| in | isEid |
ID is extended or not. |
| in | data |
Pointer to the message to send. |
| in | length |
Length of the message to send. |
if message was transmitted successfully or not. |