7.6.10 Wake-up Signal Characteristics and Timing - Rev C2

Note: This section describes the timing and behavior for LAN8670/1 revision C2 and earlier.

The following diagram illustrates the behavior and timing characteristics as the device wakes from sleep.

Figure 7-14. Wake Signal Timing (Rev C2)
Table 7-20. 10BASE-T1S PMA Receiver Wake Signal Characteristics (Rev C2)
DescriptionSymbolMin TypMaxUnits

Additional
Information

MDI wake response timetdet_mdi250450μsNote 1
MDI wake signal thresholdVthresh_mdi100700mVppNote 2
Note:
  1. The device will not wake if the signal duration is less than or equal to the minimum value of tdet_mdi. It will wake if the signal duration is greater than or equal to the maximum value of tdet_mdi. The behavior is undefined for signal duration between these limits.
  2. The device will not wake if the signal amplitude is less than or equal to the minimum Vthresh_mdi. It will wake if the signal amplitude is greater than or equal to the maximum value Vthresh_mdi. The behavior is undefined for amplitudes between these limits.
Table 7-21. WAKE_IN Signal Characteristics (Rev C2)
DescriptionSymbolMin TypMaxUnits

Additional
Information

WAKE_IN response timetdet_wi3340μsNote 1
WAKE_IN detection timetdet_wi_vld152240μsNotes 2, 3
Note:
  1. Measured from WAKE_IN active edge to INH assertion.
  2. The device will not wake if the signal duration is less than or equal to the minimum value of tdet_wi. It will wake if the signal duration is greater than or equal to the maximum value of tdet_wi. The behavior is undefined for signal duration between these limits.
  3. The WAKE_IN pin is a standard VI-VDDAU type input buffer. See the section DC Electrical Characteristics (other than 10BASE-T1S PMA) for details.
Table 7-22. Wake Signal Time (Rev C2)
DescriptionSymbolMinTypMaxUnits

Additional
Information

IRQ_N assertion time after all power supplies validtpo_irq6.6μs

MDI wake forward signaling activity start after all power supplies valid

tpo_mdi2μs

WAKE_OUT wake forward assertion time after all power supplies valid

tpo_wo1.8µs
WAKE_OUT pulse widthtwo90μs
MDI wake signaling timetwk_mdi1ms
Power supply response timetps_respApplication SpecificNotes 1, 2
Note:
  1. The power supply response time is the length of time from the power supplies being enabled by INH being driven high to the time the VDDP and VDDA supplies are high enough to release the internal power-on reset circuits. This time is dependent upon the implementation of the external power supply circuits and therefore is implementation specific.
  2. The VDDP and VDDA supplies must be disabled after entering sleep mode prior to a wake event.