PKOB4 and MCP2200 USB devices are accessible to the upstream PC via a common USB connector (J100) using the Microchip USB 2.0 High-Speed Hub Controller USB2512B providing the user with more ease of use.
After plugging the PIC32 BZ6 Curiosity Board into the upstream PC using a USB cable, device enumeration is as illustrated in the following figure for the PKOB4 and MCP2200.Figure 3-4. Device Manager
DS00006006C
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.