21.5.2 remove_hdl_core
(Ask a Question)Description
This Tcl command removes and HDL core component from the current project. The command will fail if the module name is not specified or is incorrect.
remove_hdl_core -hdl_core_name { hdl_core_name }
Arguments
Parameter | Type | Description |
---|---|---|
hdl_core_name |
string |
Specify the module name from which you want to delete a core component. This is a mandatory argument. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None |
Required parameter 'hdl_core_name' is missing. |
None |
Parameter 'param_name' is not defined. Valid command formatting is ' remove_hdl_core -hdl_core_name "hdl core name"'. |
Supported Families
PolarFire® |
PolarFire SoC |
SmartFusion® 2 |
IGLOO® 2 |
RTG4™ |
Example
The following example removes 'test_hdl_core' HDL core component:
remove_hdl_core -hdl_core_name {test_hdl_core}