8.2 Fold Instance

The expanded hierarchy of an instance can be folded or collapsed back into the parent instance.

Use one of the following three ways to fold/collapse the expanded instance back into the parent instance:

  • Click the - button at the top left of the instance.
    Figure 8-34. Fold Instance Icon
  • Click to select the expanded instance, then right click and select Fold Instance in the menu.
    Figure 8-35. Fold Instance Menu Item
  • Click the Fold All Instance icon.