8.2 Expand InPlace

Use one of the following two ways to execute the Expand Inplace operation on an instance.

  • Click the + button at the top left of the instance, which indicates that it is pushable.
Figure 8-32. Expand in Place icon
  • Left click to select the instance and then right click to select Expand Inplace.
Figure 8-33. Expand Inplace Menu Selection